STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8S103 not understanding interrupt priority.

Hi,I do not grasp the STM8S103 interrupt priority philosophy. Each Io-port can be assigned to 1 out of 4 priority levels called level 0, 1, 2 and 3 page 68/467 of the RM0016 reference manual meaning highest number is handled first. I connect a slow s...

sthvw by Associate III
  • 1523 Views
  • 2 replies
  • 0 kudos

Resolved! programming STM8S103 through ST-Link V2

ST VP Configuration - ST-Link - USB - SWIM - STM8S103F3I have connected the "SWIM" and "GND" pins of 'ST-LINK V2' to the development PCB includes "STM8S103F3", the supply from the mobile charger is connected through the USB port of the PCB.When I sel...

Resolved! Logic for checksum of s19 file in stm8 stvp

Hello. I am trying to modify my s19 file which is generated for stm8 using stvd and cosmic c compiler. Consider an S19 file which starts from 0x4000 address [EEPROM starting address]The first two lines would be : S123400000000000000000000000000000000...

raja1 by Associate II
  • 2126 Views
  • 3 replies
  • 1 kudos

Resolved! Marking STM8L151F3U6TR

Hi, I have bought the parts STM8L151F3U6TR. The marking indicated in datasheet is L526. However, marking on component is L536. Anyone can confirm this marking of L536 is correct? 

Unknown TSSOP-20 chip identification

Hi all.I'm struggling with certain device and I'd like to identify unknown TSSOP-20 chip on the PCB. Chip must be an MCU and based on the pinout it's very close to some STM8, eg. STM8AF6213. There are VCC and GND connected to Pin 9 and 7 respectively...

MPrih.1 by Associate
  • 2857 Views
  • 4 replies
  • 0 kudos

IWDG STM8

Hello,STM8S208RB microcontroller, Independent watchdog (IWDG). After starting the watchdog timer (command KEY_ENABLE value = 0xCC), I understand that the watchdog timer stops after resetting the microcontroller. The default register state is undefine...

MykolaLevun_0-1707560153755.png

My first ever PCB design. Any comments? Tips or tricks?

Hello stm community. I am designing my first ever PCB board and i need some comments of yours. Here is the screenshots of the pcb schematic and pcb itself. Do you see any mistakes etc? Also I am not sure about the VCAP connection. Is it correctly mad...

Screenshot 2024-01-21 154527.png Screenshot 2024-01-21 154550.png Screenshot 2024-01-21 154605.png Screenshot 2024-01-21 154617.png
bepo-san by Associate II
  • 5903 Views
  • 12 replies
  • 5 kudos

STM8S005K6T6 needs working within 10ms

 Hello everyone!I have a question and seek your help: I ​​use STM8S005K6T6 microcontroller and cc1101 RF transceiver module, and the operation at 433 MHz is affected. It generates power automatically and can only last for 10ms. The voltage remains at...

Emanuel_ by Associate
  • 1450 Views
  • 1 replies
  • 0 kudos

STM8L101F2 consumption in Halt mode

Hi,i have STM8L101F2 at breadboard. Decoupling capacitors 100nF+22uF, supply voltage 3.3V from linear lab.power supply, nothing connected to any pin. Simple firmware (Cosmic compiler)void main(void){ GPIO_Init(GPIOA, GPIO_Pin_All,GPIO_Mode_In_PU_No...

Resolved! How STM8S001J3 use BOR function?

Hello. I am using the STM8S001J3 MCU. I want to use the reset function in my MCU. stm8 has a total of 9 Reset functions.●External reset through the NRST pin● Power-on reset (POR) and brown-out reset (BOR): During power-on, the POR keeps the device un...