STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Error : SWIM prog error[42007] buffer program error

When we debug with ST-link/V3set on STVD, we found this issue swim prog error[42007] buffer program error.but we didn't found this issue with ST-link/V2.How does solve this issue when we used the ST-link/V3set ?

CChie.6 by Associate
  • 607 Views
  • 0 replies
  • 0 kudos

With the STM8s105c6 and the STM8af5288tay, both which I use. what is the correct way to initialize multiple i2c devices on the same SDA/SCL port. i.e. I wish to have a RTC, i2c LCD as well as an EEPROM on the same i2c port.

How for example do I initialize all 3 devices, where addressing and necessary parameters are concerned.  Any sample code or advice in this regard would be very welcome. (RTC : either PCF8563 or DS1307; I2C LCD with PCF8574 expander and 24c32 or 24c64...

MGoss.19 by Associate
  • 654 Views
  • 0 replies
  • 0 kudos

Error creating process for executable cxstm8

I'm using the Cosmic Software 4.4.9.0 in ST Visual Develop 4.3.12  I can't compile it.I try to install again but it showing same error.i tried to set root path correct like this C:\Program Files\COSMIC\FSE_compilers\CXSTM8.Can any one help me to solv...

tvenk by Associate II
  • 1865 Views
  • 1 replies
  • 0 kudos

Jump to code in RAM

In the documentation for switching to low power run mode it mentions that you need to jump to code in RAM before shutting down the FLASH.How do you specify that code should be placed in RAM?OK Update:This is for the STM8L151F3.I found link to a sugge...

TVan.11 by Associate
  • 495 Views
  • 0 replies
  • 0 kudos

STM8: mistake in datasheet?

Good morning.STM8S003: https://www.st.com/resource/en/datasheet/DM00024550.pdfOn a page 45 under table 15 (quote):"2. Do not use more than one remapping option in the same port. It is forbidden to enable both AFR1 and AFR0."Here first part of the sen...

Arlleex1 by Associate III
  • 487 Views
  • 1 replies
  • 0 kudos

Hi, I have Design a Relays Based AC Switch Board using STM8s003 and ESP01. When I connect even a small resistive load then the controller resets during relays switching.... i dont know whether where is the problem in my design?

 >>The Board is working fine when there is no AC (220v) load Connected; but with AC Load Connected, then MCU resets during switchingSame type of switch boards are available online containing stm8 but i havent experienced these boards regarding such a...

SKhan.4 by Associate
  • 651 Views
  • 0 replies
  • 0 kudos