2012-06-12 06:06 AM
Hello,
STM8L specifies 4 types of input pins (Table 34. I/O static characteristics): - True open-drain pins (PC0 and PC1) used for I2C - Five-volt tolerant pins (PA7 and PE0) - 3.6 V tolerant - Any other pins Which pins are the 3.6V tolerant ones? And does this mean the pins can withstand 3.6V even if VDD is 1.8V? Thanks for any clarification... #stm8l-inputs