cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 external loader program with STM32Cube programmer

Hello, I build program to store data in external QSPI flash memory using STM32Cube programmer and generated .stldr file but as soon as I place same file to bin external loader folder (STM32Cube\STM32CubeProgrammer\bin\ExternalLoader), STM32Cube programmer IDE wouldn't open. I not able to find the reason. Any suggestions?

Attaching my project.

Thanks

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11

@Community member​  Thanks you taking out your time.

I am agree. There should be error handling in STM32 Cube Programmer. Its like black box right now. i spent so much of my time in just adding *.stldr file to it.

-Chandan

I am able to load *.stldr file in STMCube programmer and able to mass erase but Facing below issue when programming,

12:45:30 : STM32CubeProgrammer API v2.4.0

12:45:30 : ST-LINK error (DEV_CONNECT_ERR)

12:45:37 : ST-LINK SN : 066FFF545554827867064115

12:45:37 : ST-LINK FW : V2J33M25

12:45:37 : Voltage : 3.21V

12:45:37 : SWD freq : 4000 KHz

12:45:37 : Connect mode: Normal

12:45:37 : Reset mode : Software reset

12:45:37 : Device ID : 0x449

12:45:38 : UPLOADING OPTION BYTES DATA ...

12:45:38 : Bank : 0x00

12:45:38 : Address : 0x40023c14

12:45:38 : Size : 8 Bytes

12:45:38 : UPLOADING ...

12:45:38 : Size : 1024 Bytes

12:45:38 : Address : 0x8000000

12:45:38 : Read progress:

12:45:38 : Data read successfully

12:45:38 : Time elapsed during the read operation is: 00:00:00.007

12:45:49 : Memory Programming ...

12:45:49 : Opening and parsing file: MyDevKitProj.elf

12:45:49 : File : MyDevKitProj.elf

12:45:49 : Size : 967244 Bytes

12:45:49 : Address : 0x08000000 

12:45:49 : Erasing memory corresponding to segment 0:

12:45:49 : Erasing internal memory sectors [0 4]

12:45:51 : Erasing memory corresponding to segment 1:

12:45:51 : Erasing external memory sectors [0 11]

12:45:52 : Download in Progress:

12:46:03 : Error: failed to download Segment[1]

12:46:03 : Error: failed to download the File

12:46:03 : RUNNING Program ... 

12:46:03 : Address: : 0x08000000

12:46:03 : Application is running

12:46:03 : Start operation achieved successfully

From log it seems like, Programmer is able to erase sectors but unable to write it.

When I called SectorErase() and Write() functions from normal program in main, I can see data is able to store at external QSPI flash. Not sure about STMCube programmer issue.

uint8_t CSP_QSPI_WriteMemory(uint8_t* buffer, uint32_t address,uint32_t buffer_size) {

QSPI_CommandTypeDef sCommand;

uint32_t end_addr, current_size, current_addr;

/* Calculation of the size between the write address and the end of the page */

current_addr = 0;

//

while (current_addr <= address) {

current_addr += MEMORY_PAGE_SIZE;

}

current_size = current_addr - address;

/* Check if the size of the data is less than the remaining place in the page */

if (current_size > buffer_size) {

current_size = buffer_size;

}

/* Initialize the adress variables */

current_addr = address;

end_addr = address + buffer_size;

sCommand.InstructionMode = QSPI_INSTRUCTION_1_LINE;

sCommand.AddressSize = QSPI_ADDRESS_24_BITS;

sCommand.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;

sCommand.DdrMode = QSPI_DDR_MODE_DISABLE;

sCommand.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;

sCommand.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;

sCommand.Instruction = QUAD_IN_FAST_PROG_CMD;

sCommand.AddressMode = QSPI_ADDRESS_1_LINE;//QSPI_ADDRESS_4_LINES; //

sCommand.DataMode = QSPI_DATA_4_LINES;

sCommand.NbData = buffer_size;

sCommand.Address = address;

sCommand.DummyCycles = 0;

/* Perform the write page by page */

do {

sCommand.Address = current_addr;

sCommand.NbData = current_size;

if (current_size == 0) {

return HAL_OK;

}

/* Enable write operations */

if (QSPI_WriteEnable() != HAL_OK) {

return HAL_ERROR;

}

/* Configure the command */

if (HAL_QSPI_Command(&hqspi, &sCommand, HAL_QPSI_TIMEOUT_DEFAULT_VALUE)

!= HAL_OK) {

return HAL_ERROR;

}

/* Transmission of the data */

if (HAL_QSPI_Transmit(&hqspi, buffer, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK) {

return HAL_ERROR;

}

/* Configure automatic polling mode to wait for end of program */

if (QSPI_AutoPollingMemReady() != HAL_OK) {

return HAL_ERROR;

}

/* Update the address and size variables for next page programming */

current_addr += current_size;

buffer += current_size;

current_size =

((current_addr + MEMORY_PAGE_SIZE) > end_addr) ?

(end_addr - current_addr) : MEMORY_PAGE_SIZE;

} while (current_addr <= end_addr);

return HAL_OK;

}