cancel
Showing results for 
Search instead for 
Did you mean: 

STLink V3 CANBUS bootloader over STM32CubeProgrammer problem

Linas L
Senior II

Hello,
In one of my boards I was planing to use CANBUS bootloader and STLink V3 with external canbus PHY to program MCU.

I was unable to program it, I can see STlink V3 does try to do some TX on CANBUS pin, but where is no packet available that could be decoded, just train of same duty cycle pulses.

Does any one had luck with STLink V3 and external CANBUS programming ? What I am doing wrong ?

  • Yes, I added external TCAN1462VDRBRQ1 IC for programmer, and connected to RXD and TXD pins on STLINKV3_MDOS (RX 9, TX 10pin)
  • Yes, I enabled externally TCAN1462VDRBRQ1 to be in active mode all the time
  • Yes, I placed BOOT0 pin to high level when connecting power (same pin for power and BOOT)
  • YES, STM32U585 uses PB8+PB9 as per datasheet for canbus bootloader

CANBUS_MDOS.PNGCAN_PHY.PNG

BOOT.PNG

STLink.PNG

 

15 REPLIES 15

What did you end up doing? coding your own FDCan bootloader host? or downgrading to classic can?

hit me up in https://www.linkedin.com/in/javiermu%C3%B1oz/

I tested FDCAN bootloader, and it works with my own FDCAN controller, but not programmer. This is not that hard to implement, just like UART or any other bootloader.

Question do you have tools for it.

Alright so you ended up creating your own FDCAN bootloader

hit me up in https://www.linkedin.com/in/javiermu%C3%B1oz/

Well, not exactly, I was using internal bootloader with another STM32H7 that is controlled over USB to flash firmware over canbus.

So flash handling is done via STbootloader on U5 device, but commands are send via STM32H7 with windows controlling it


@Linas L wrote:

I tested FDCAN bootloader, and it works with my own FDCAN controller, but not programmer.


This seems to be a known limitation of CubeProgrammer (or, rather, ST-Link V3):

https://community.st.com/t5/stm32cubeprogrammer-mcus/accessing-fdcan-system-bootloader-with-stlink-v3-cubeprogrammer/m-p/764176/highlight/true#M7728

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

could you share your wiring with STLNK-v3 and CANPHY?

hit me up in https://www.linkedin.com/in/javiermu%C3%B1oz/