cancel
Showing results for 
Search instead for 
Did you mean: 

STLink V2 Not recognizing STM32CubeProgrammer? UR connection mode is defined with the HWrst reset mo

zachary.cain
Associate II

zacharycain_0-1691599853462.png

ST Link not recognizing STM Cube Programmer? - From screenshot you can see pulls up single character serial number and has no target information. I can (and did) upgrade firmware to latest on ST Link. Downloaded all drivers etc. Still won't connect. Keep getting "UR connection mode is defined with the HWrst reset mode" log entry.

 

 

 

14 REPLIES 14
Pavel A.
Super User

@SBenn.2 The serial number on your screenshot is not 1-character. ???

Yes that's right, I only included the screen shot after the SHARED option is ticked, without being ticked the fake ST-Link is not detected in any way in CubeIDE i.e. not even showing the ! character, this is where it is different from CubeProgrammer, which does show an ! as the serial number, if not shared.

APuht
Associate II

I had the same problem. Instead of the serial number, "C" was displayed. In the cube programmer I set the "Shared" option to Enable and everything worked.

After installing the utility, it is showing this error

  • The code execution cannot proceed because mfc140.dil was not found.

Thankyou zachary.cain, I have followed your suggestion and it works.