cancel
Showing results for 
Search instead for 
Did you mean: 

Reprogramming of the STM32H743zi2 board

mvenkat86
Associate II

Hi,

I have erased the program in the chip by pressing erase program in the STM32Cub programmer, now the board is not working , Can you please support on this issue?

 

 

 

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Issamos
Lead III

Hello @mvenkat86 

Do you have the same problem as this post. If no, could you provide more details (error notifications, screenshots, ...).

Best regards.

II 

TDK
Super User

What does not working mean here? If you erase the flash, the program isn't going to do what it used to do.

If you feel a post has answered your question, please click "Accept as Solution".
FBL
ST Employee

Hello @mvenkat86 

It is possible that you are booting from system memory! Have you changed the boot address option byte?

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL