Skip to main content
Associate II
October 2, 2024
Question

Installing SFI remotely on NUCLEO-U575ZI-Q

  • October 2, 2024
  • 1 reply
  • 620 views

Hi,

I have generated a SFI file and managed to install it on my NUCLEO-U575ZI-Q using STM32CubeProgrammer. Now, as a next step, I want to install this SFI file remotely (e.g. on another PC or similar), is there any way to do this installation, or does it have to be connected to a PC that has STM32CubeProgrammer? Either via SSH or something similar.

Best regards and thanks in advance.

This topic has been closed for replies.

1 reply

Visitor II
October 5, 2024

@mikel-mehall wrote:

Hi,

I have generated a SFI file and managed to install it on my NUCLEO-U575ZI-Q using STM32CubeProgrammer. Now, as a next step, I want to install this SFI file remotely (e.g. on another PC or similar), is there any way to do this installation, or does it have to be connected to a PC that has STM32CubeProgrammer? Either via SSH or something similar.

Best regards and thanks in advance.


To install the SFI file remotely on your NUCLEO-U575ZI-Q, you typically need a method to flash the firmware without being directly connected to a PC running STM32CubeProgrammer. While STM32CubeProgrammer is primarily designed for local installations. Hope! it would be helpful.