cancel
Showing results for 
Search instead for 
Did you mean: 

External Flash Loader gets "failed to download Segment[0]" error on STM32CubeIDE

ARost.9
Associate III

Hello, I have made a custom external flash loader(.stldr) file for my STM32 based board and this file works great with ST Link Utility(Read, Write and Erase) are work fine and i can Program the board correctly. But when i try to use the created .stldr file by STM32CubeIDE the erasing process well done but when the downloading process gets start then "failed to download Segment[0]" error pups up.

Could any one help me with the problem?

MCU = STM32H743iit6

QSPI Flash = W25Q256

 
STMicroelectronics ST-LINK GDB server. Version 6.0.0
Copyright (c) 2021, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
        Persistent Mode            : Disabled
        Logging Level              : 1
        Listen Port Number         : 61234
        Status Refresh Delay       : 15s
        Verbose Mode               : Disabled
        SWD Debug                  : Enabled
        InitWhile                  : Enabled
 
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
      -------------------------------------------------------------------
                       STM32CubeProgrammer v2.9.0-RC01                  
      -------------------------------------------------------------------
 
ST-LINK SN  : 48FF6D068366565223471581
ST-LINK FW  : V2J39S7
Board       : --
Voltage     : 3.24V
SWD freq    : 4000 KHz
Connect mode: Under Reset
Reset mode  : Hardware reset
Device ID   : 0x450
Revision ID : Rev V
Device name : STM32H7xx
Flash size  : 2 MBytes
Device type : MCU
Device CPU  : Cortex-M7
BL Version  : 0x90
 
 
 
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a23188.srec
  File          : ST-LINK_GDB_server_a23188.srec
  Size          : 389352 Bytes
  Address       : 0x08000000 
 
 
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Erasing memory corresponding to segment 1:
Erasing external memory sectors [0 3]
Download in Progress:
 
 
Error: failed to download Segment[0]
Error: failed to download the File
Shutting down...
Exit.

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12

There's another thread discussing the replacement of the INTERNAL loader with one from the 2.6.0 era to resolve an issue like this.

I​ can't say I've needed it for my H7 loaders, but that might relate to my strategy.

I'll get you a cite when I'm at a computer. Look at post history for @N. SANTINI​ ​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

https://community.st.com/s/question/0D53W00001cIHMQSA4/external-loader-fails-to-download

The loaders I've been building are posted here

https://github.com/cturvey/stm32extldr

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Roberto C
Associate III

Ok, Thnx for suggestions!