2025-05-18 8:52 AM
Hello,
I'd like to ask if there are plans to implement SWO support in Cube Programmer API? I would be very helpful to read the SWO ouput directly using the C++ API, not by using CLI.
2025-05-18 10:27 AM
A driver that exports it as COM port, a Filter Driver or firmware that creates a USB CDC/VCP would also simplify connectivity and automation using existing interfaces and methods..
2025-05-18 12:14 PM - edited 2025-05-26 12:22 AM
Hello @Wasilewski.Piotr @Tesla DeLorean
Thank you for your suggestions. I've escalated this to the concerned team to see the possibility to implement it on the future (under internal ticket number 210736).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.