cancel
Showing results for 
Search instead for 
Did you mean: 

Will pre-C5 series (like F4) be compatible with CubeMX2 and HAL2?

llLeo306
Associate

Hi everyone,

I have a quick question regarding the upcoming release of CubeMX2 and its backward compatibility.

Once CubeMX2 is released, will the older series before C5 (like the F4) support MX2 and HAL2?

Also, if they do support it, will we be forced to bundle HAL2 for these older models, or will there be some flexibility?

Thanks in advance for any insights or official clarification!

Best,
Leo

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello @llLeo306 and welcome to the ST community,

Older MCU series remain in HAL/MX while new series will come with HAL2/MX2.

No plan for the moment to migrate old series to HAL2/MX2.

Both flavors will be supported in the same way.

I can't tell more.

Hope that answers your question.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
mƎALLEm
ST Employee

Hello @llLeo306 and welcome to the ST community,

Older MCU series remain in HAL/MX while new series will come with HAL2/MX2.

No plan for the moment to migrate old series to HAL2/MX2.

Both flavors will be supported in the same way.

I can't tell more.

Hope that answers your question.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.