cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U5A5 Nucleo, issue with CubeMX warning related to RCC and PWR setting

Riscy
Senior

I have Nucleo STM32U5A5 board where I experiment with the USBX interface based on demo code. I then created new project to experiment with GPDMA. Both IDE and MX are updated at the time of 30/Nov/23. 

It keep on repeating RCC/PWR setup warning or issue when I run generate code. When I went back to demo code: Ux_Device_CDC_ACM, I also generated the code from CubeMX with added USART2. It produce same RCC/PWR error. It seen to point to PWR privilege and RCC privilege (with !) on it. I have not activated trustzone. 

Can you advise what should I do about it, is there bug in these or workaround?

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
Riscy
Senior

Any progress for a solution?

Riscy
Senior

Any other suggestion, has this bug been reported?