cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-G070RB ADC not working channels 2 to channel 5

Chinna651302
Associate

Title edited to reflect that this relates specifically to the NUCLEO-G070RB board.


NUCLEO-G070RB in this board  ADC channel 0,1 working ,other ADC channel not working is they any reason?

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @Chinna651302, to the community!

If you look at the schematics of the NUCLEO_G070RB, you will see that the associated pins PA2, PA3 and P5 are already in use, but ADC_IN4 = PA4 is free and should therefore work as an ADC input. Unfortunately, no alternative pins are available for the ADC inputs, so on the NUCLEO you cannot use ADC_IN2, ADC_IN3 and ADC_IN5 without changing the components that are already connected.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome @Chinna651302, to the community!

If you look at the schematics of the NUCLEO_G070RB, you will see that the associated pins PA2, PA3 and P5 are already in use, but ADC_IN4 = PA4 is free and should therefore work as an ADC input. Unfortunately, no alternative pins are available for the ADC inputs, so on the NUCLEO you cannot use ADC_IN2, ADC_IN3 and ADC_IN5 without changing the components that are already connected.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello @Peter BENSCH ,

 

Thank you for your prompt response. I reviewed the schematics and was able to identify the issue. I appreciate your clear explanation and valuable suggestions.
 
Regards,
Chinna