cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F303CCT6 - STM32CubeF3.1.2.0

George.P
Associate III
Posted on September 04, 2015 at 15:00

Hello,

I'm having problems initializing the CAN peripheral, using generated code by Cube.

APB1 Peripheral clock is 32MHz (XTAL16*PLL4*0.5PRESC).

The device cannot get INAK cleared after clearing INRQ.

Pins seem to be correctly set up on the alternate function (Mode = AF_PP and Alternate = AF9_CAN).

Any help would be great!

Here are some code snippets.

void MX_CAN_Init(void)

{

  hcan.Instance = CAN;

  hcan.Init.Prescaler = 8;

  hcan.Init.Mode = CAN_MODE_NORMAL;

  hcan.Init.SJW = CAN_SJW_1TQ;

  hcan.Init.BS1 = CAN_BS1_8TQ;

  hcan.Init.BS2 = CAN_BS2_7TQ;

  hcan.Init.TTCM = DISABLE;

  hcan.Init.ABOM = DISABLE;

  hcan.Init.AWUM = DISABLE;

  hcan.Init.NART = DISABLE;

  hcan.Init.RFLM = DISABLE;

  hcan.Init.TXFP = DISABLE;

  HAL_CAN_Init(&hcan);

}

void HAL_CAN_MspInit(CAN_HandleTypeDef* hcan)

{

  GPIO_InitTypeDef GPIO_InitStruct;

  if(hcan->Instance==CAN)

  {

  /* USER CODE BEGIN CAN_MspInit 0 */

  /* USER CODE END CAN_MspInit 0 */

    /* Peripheral clock enable */

    __CAN_CLK_ENABLE();

  

    /**CAN GPIO Configuration    

    PB8     ------> CAN_RX

    PB9     ------> CAN_TX 

    */

    GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9;

    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

    GPIO_InitStruct.Pull = GPIO_NOPULL;

    GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;

    GPIO_InitStruct.Alternate = GPIO_AF9_CAN;

    HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

  /* USER CODE BEGIN CAN_MspInit 1 */

  /* USER CODE END CAN_MspInit 1 */

  }

}

/* Request leave initialisation */

    hcan->Instance->MCR &= ~(uint32_t)CAN_MCR_INRQ;

    /* Get timeout */

    tickstart = HAL_GetTick();   

   

    /* Wait the acknowledge */

    while((hcan->Instance->MSR & CAN_MSR_INAK) == CAN_MSR_INAK)

    {

      if((HAL_GetTick()-tickstart) > INAK_TIMEOUT)

      {

         hcan->State= HAL_CAN_STATE_TIMEOUT;

         return HAL_TIMEOUT;

      }

    } 

#stm32f3-can-cubemx
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
George.P
Associate III
Posted on September 08, 2015 at 07:12

The problem was solved kind of its own when I connected the power pin on the external CAN  transceiver.

It seems that the CAN peripheral refuses to leave initialization if the associated pin logic state does not match normal operation values, i.e. the CAN transceiver has to be powered on.

Ankit Rathore
Associate
Posted on May 04, 2017 at 08:23

Hi All,

      i am using STM32F303RE my code also stuck at this function :-  

     while((hcan->Instance->MSR & CAN_MSR_INAK) == CAN_MSR_INAK)

{

if((HAL_GetTick()-tickstart) > CAN_TIMEOUT_VALUE)

{

hcan->State= HAL_CAN_STATE_TIMEOUT;

/* Process unlocked */

__HAL_UNLOCK(hcan);

return HAL_TIMEOUT;

}

}

i am using default code with certain pin changes (PIN are correct i crosscheck  )

Please help, i will have to deliver this with in 2 day.

Thanks

Ankit Rathore