2025-04-16 12:53 AM
2025-04-16 3:24 AM
Hello @STxuetu
Could you please try to delete \.stm32cubemx folder and check!
Otherwise, could you check if some antivirus/firewall is activated?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-16 1:39 AM
Hello @STxuetu
Could you provide further information on the CubeMX version and OS you are using?
BR,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-16 2:04 AM
i7-12700H 2.30 GHz,64-bit operating system, x64-based processor
STM32CubeMX-6.14.1
2025-04-16 2:05 AM
After the first installation, you can open it once, close it and it will not open
2025-04-16 2:36 AM
i7-12700H 2.30 GHz,64-bit operating system, x64-based processor STM32CubeMX-6.14.1After the first installation, you can open it once, close it and it will not open
2025-04-16 3:24 AM
Hello @STxuetu
Could you please try to delete \.stm32cubemx folder and check!
Otherwise, could you check if some antivirus/firewall is activated?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-16 7:20 PM
Hi, I followed your instructions and deleted the \.stm32cubemx folder and was able to open cubemx successfully.
I'd like to ask if the deleted folder is redundant, I'd appreciate your guidance on this