cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX V4.27.0 release note states that STM32H7 uses firmware V1.4.0. Whereas in reality it uses V1.3.0.

MaxR
Associate II

STM32CubeMX V4.27.0 release note states that STM32H7 uses firmware V1.4.0. Whereas in reality it uses V1.3.0. Is it possible to download STM32H7 firmware V1.4.0. I could not find it anywhere. Is firmware update planed?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Houda GHABRI
ST Employee

Hello @MaxR​  ,

We are sorry, there is a typo in Release note of STM32CubeMX 4.27.0 , STM32H7 use V1.3.0 and not 1.4.0.

It is not possible to download the H7 FW 1.4.0 because it is not yet available :) but update is planned for the future.

Regards,

Houda

View solution in original post

3 REPLIES 3
Khouloud GARSI
ST Employee

Hi @MaxR​ ,

The STM32H7 uses STM32Cube firmware V1.3.0. This is a typo in the release note which will be fixed in the next update of the document.

Thanks for bringing this point to our attention.

Khouloud.

>>Is firmware update planed?

It is, but there isn't a schedule, and current release supports the NUCLEO/EVAL boards fully

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Houda GHABRI
ST Employee

Hello @MaxR​  ,

We are sorry, there is a typo in Release note of STM32CubeMX 4.27.0 , STM32H7 use V1.3.0 and not 1.4.0.

It is not possible to download the H7 FW 1.4.0 because it is not yet available :) but update is planned for the future.

Regards,

Houda