cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX - Could not create a project for the STM32MP2

pp24
Visitor

Hello,

I’m unable to create a new project for the STM32MP2 (STM32MP251CAL3) in STM32CubeMX (Version 6.14.1). After selecting the MPU and clicking Start Project, I choose the TrustZone feature—but nothing happens. I can see a “*” appear next to “Untitled” in the top left, but no further dialog appears.

When I try to select an MCU, I receive the warning:

“Project Untitled has been modified would you like to save the projekt?”

If I click Yes, the mouse cursor turns into the blue loading spinner and nothing else happens.

In the Output window, I see:

 Creating: STM32MP251CALx

 Initializing: STM32MP251CALx

 Environment: STM32CubeMX

 

2025-05-05 15_40_18-STM32CubeMX Untitled_.png

 

Even when editing an existing project, I can click options in Pinout & Configuration, but the cursor just shows the blue loading spinner and nothing else occurs.

2025-05-05 15_42_19-STM32CubeMX STM32MP2.ioc__ STM32MP251CALx.png

Could you please help me resolve this?

2 REPLIES 2
Mahmoud Ben Romdhane
ST Employee

Hello @pp24 ,

 

First let me thank you for posting and welcome to the ST Community.

I am not able to reproduce the behavior that you described.

I suggest that you provide more details such as the Ioc and the log file.

 

Thanks.

Mahmoud

Hello @Mahmoud Ben Romdhane ,

 

Thank you for the quick reply.

I can't provide the IOC at the moment, but it's mainly about creating a new one.

 

Regards,

Philipp