cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 4.3.0 : delete user files in project folder

gk
Associate II
Posted on July 07, 2014 at 13:26

Hi,

Up to MX 4.2.0 it newer happends, but after upgrade MX to 4.3.0 time to time all user project  files are deleted in project folder!. STM32CubeF4  1.3.0

Windows 7 x64,  Eclipse 4.3.2 + STM32CubeMX 4.3.0 plugin.

It quite offten - after regenerate project all files created not by STM32Cube are gone!

Anybody can confirm that?

SOLVED:

Before regeneration I alwas save project using icon with two disc - now is ''Save the Project in a new file''.

AFAIR always done that and I sure before works different way - not delete user files

-------------------------------------------------------

From MX 4.3.0

''Save the current Project'' (one disc icon) keeps user files

''Save the Project in a new file'' (two disc icon) delete all - include user files and create project from begining

-------------------------------------------------------

maybe it helps for someone

Regards

#stm32cubemx-4.3.0
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
stm32cube-t
ST Employee
Posted on November 03, 2014 at 11:05

Dear user,

Sorry for this issue. Please upgrade to latest 4.4 release.

Thank you.