2025-04-24 7:39 PM
I met a problem when using CubeMX to modify the CSI to start the camera module, but it shows that the CSI cannot be adjusted correctly. I want to know how to solve this problem.
Solved! Go to Solution.
2025-04-25 7:19 AM
Hello @Z-YF
Since Version 6.14.1 of CubeMX, you can only activate CSI mode by setting the CSI peripheral. However, to configure the parameters of CSI, go to Serial Interface Configuration under DCMIPP.
BR,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-25 3:41 AM
Hello @Z-YF
Are you using STM32CubeMX V6.14.1 ?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-25 3:47 AM
Yes.
2025-04-25 7:19 AM
Hello @Z-YF
Since Version 6.14.1 of CubeMX, you can only activate CSI mode by setting the CSI peripheral. However, to configure the parameters of CSI, go to Serial Interface Configuration under DCMIPP.
BR,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-25 8:46 AM
OK, I fixed it.
Thank you for your time. :)