2021-10-19 4:59 AM
Hi - I'm working on some projects with STM32CubeIDE (1.6.1) and CubeMX (). What I've noticed is that if I generate a CubeMX project targeting a Makefile build the linker directive that is generated has some non-trivial differences with the .ld generated for a STM32CubeIDE project.
Even in the header, you can see from the comment:
** Author : Auto-generated by System Workbench for STM32that the tool is generating an outdated ld. If you diff the two files, you'll see how _estack is defined is different, there are many missing ALIGN(4); calls, RamFunc is missing, etc.
I think this is just an oversight, and should be corrected in the next build of CubeMX/CubeIDE.