cancel
Showing results for 
Search instead for 
Did you mean: 

How to solve the problem? STM32CubeMX 5.0.0 These IPs still have some not configure or wrong parameter values:[FATFS]

QSiji
Associate

The project was create in CubeMX of earlier verson 4.29.0 , and it can easily to generate code. But a couple of days earlier, I need to add a new pin to the project. So I added the pin configure in CubeMx of Verson 5.0.0. When I generate codes, tips above happens. So how to solve the problem.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
hwen
Associate

Set an input pin and select that input pin.