cancel
Showing results for 
Search instead for 
Did you mean: 

Help Needed: Setting Up CLion for STM32 Development on macOS

lalalala
Associate II

Hi everyone,

 

I’m new to STM32 development and need some help configuring CLion for working with STM32 microcontrollers. I have installed STM32CubeMX (version 6.13.0) and am trying to generate a project for my STM32F411CEU6 microcontroller. However, I’m encountering an issue where the Eclipse launcher fails to work, and I can’t proceed further.

 

I’m using macOS Sequoia (version 15.2). Could anyone guide me through the process of setting up CLion on macOS to work with STM32?

 

Any advice, steps, or resources would be greatly appreciated!

 

Thanks in advance!
Screenshot 2025-01-09 at 20.18.45.pngScreenshot 2025-01-09 at 20.23.59.png

12 REPLIES 12
lalalala
Associate II

By the way, if anyone finds it useful, I’m sharing my CLion setup for STM32 development on macOS (Apple Silicon)

To get started, you’ll need to install STM32CubeCLT, which will automatically set up the required toolchain in the /opt/ directory on your Mac.

Here are screenshots of my three configurations:

Build setup

lalalala_0-1740432414728.png

Flashing the STM32

lalalala_1-1740432429031.png

Debugging setup

lalalala_2-1740432688308.png

CMakeLists.txt

 

 

set(CMAKE_SYSTEM_NAME Generic)
set(CMAKE_SYSTEM_VERSION 1)
cmake_minimum_required(VERSION 3.30)

# specify cross-compilers and tools
set(CMAKE_C_COMPILER arm-none-eabi-gcc)
set(CMAKE_CXX_COMPILER arm-none-eabi-g++)
set(CMAKE_ASM_COMPILER  arm-none-eabi-gcc)
set(CMAKE_AR arm-none-eabi-ar)
set(CMAKE_OBJCOPY arm-none-eabi-objcopy)
set(CMAKE_OBJDUMP arm-none-eabi-objdump)
set(SIZE arm-none-eabi-size)
set(CMAKE_TRY_COMPILE_TARGET_TYPE STATIC_LIBRARY)

# project settings
project(Greenhouse C CXX ASM)
set(CMAKE_CXX_STANDARD 17)
set(CMAKE_C_STANDARD 11)

#Uncomment for hardware floating point
add_compile_definitions(ARM_MATH_CM4;ARM_MATH_MATRIX_CHECK;ARM_MATH_ROUNDING)
add_compile_options(-mfloat-abi=hard -mfpu=fpv4-sp-d16)
add_link_options(-mfloat-abi=hard -mfpu=fpv4-sp-d16)

#Uncomment for software floating point
#add_compile_options(-mfloat-abi=soft)

add_compile_options(-mcpu=cortex-m4 -mthumb -mthumb-interwork)
add_compile_options(-ffunction-sections -fdata-sections -fno-common -fmessage-length=0)

# uncomment to mitigate c++17 absolute addresses warnings
#set(CMAKE_CXX_FLAGS "${CMAKE_CXX_FLAGS} -Wno-register")

# Enable assembler files preprocessing
add_compile_options($<$<COMPILE_LANGUAGE:ASM>:-x$<SEMICOLON>assembler-with-cpp>)

if ("${CMAKE_BUILD_TYPE}" STREQUAL "Release")
    message(STATUS "Maximum optimization for speed")
    add_compile_options(-Ofast)
elseif ("${CMAKE_BUILD_TYPE}" STREQUAL "RelWithDebInfo")
    message(STATUS "Maximum optimization for speed, debug info included")
    add_compile_options(-Ofast -g)
elseif ("${CMAKE_BUILD_TYPE}" STREQUAL "MinSizeRel")
    message(STATUS "Maximum optimization for size")
    add_compile_options(-Os)
else ()
    message(STATUS "Minimal optimization, debug info included")
    add_compile_options(-Og -g)
endif ()

include_directories(Inc
        Drivers/CMSIS/Device/ST/STM32F4xx/Include
        Drivers/CMSIS/Include)

add_definitions(
        -DDEBUG
        -DSTM32F411xE
)

file(GLOB_RECURSE SOURCES
        "Startup/*.*"
        "Src/*.*"
        "Drivers/*.*"
)

set(LINKER_SCRIPT ${CMAKE_SOURCE_DIR}/STM32F411CEUX_FLASH.ld)

add_link_options(-Wl,-gc-sections,--print-memory-usage,-Map=${PROJECT_BINARY_DIR}/${PROJECT_NAME}.map)
add_link_options(-mcpu=cortex-m4 -mthumb -mthumb-interwork)
add_link_options(-T ${LINKER_SCRIPT})

add_executable(${PROJECT_NAME}.elf ${SOURCES} ${LINKER_SCRIPT})

set(HEX_FILE ${PROJECT_BINARY_DIR}/${PROJECT_NAME}.hex)
set(BIN_FILE ${PROJECT_BINARY_DIR}/${PROJECT_NAME}.bin)

add_custom_command(TARGET ${PROJECT_NAME}.elf POST_BUILD
        COMMAND ${CMAKE_OBJCOPY} -Oihex $<TARGET_FILE:${PROJECT_NAME}.elf> ${HEX_FILE}
        COMMAND ${CMAKE_OBJCOPY} -Obinary $<TARGET_FILE:${PROJECT_NAME}.elf> ${BIN_FILE}
        COMMENT "Building ${HEX_FILE}
Building ${BIN_FILE}")

 

 

 

Excellent contribution. I have a similar setup, works like a charm. CLion accelerates my production at least 4-5x and diminishes faulty SW considerably. Worth every € I paid for it.

For those interested, I use SEGGER's J-Link instead of OCD. This is the setup for using it with CLion/GDB:

Scherm­afbeelding 2025-02-25 om 10.20.03.png

Hi!
Thanks a lot for your screenshots, they were crucial to start the jump to CLion.


I however have a slight problem, i am posting here in case you had it also. (and overcame it)
i am currently developping for a F103 and a L552. I can correctly compile, flash, debug from cubeIDE on the 103 with the project as CMAKE. L552 does not work with CMake, i believe the support is not quite there yet.

However, when i try to debug, doing almost the same thing as you under Clion, the stlink (or nucleo on L552) tells me it can not find the target. Even the nucleo, which is rather weird. I can jump in immediately in cubeprogrammer or cubeide and conect to it, no worries. I can also flash without problem from CLion.

I saw you used CLT1.17, i tried it, tried the 1.21, to no better result. Still i have something weird that might be of a significant interest: the ST-LINK_gdbserver batch refuses to see the config.txt file, i resorted to add parameters to the CLion debug configuration.

Is that ringing a bell? 

Thanks a lot.