cancel
Showing results for 
Search instead for 
Did you mean: 

Confirm my STM32G070RBT6 SPI1 configuration ?

CabinJo
Visitor

Hello.

Please check if there are any issues with the settings as shown below.

PB4 : SPI1_miso

PB3 : SPI1_sck

PD6 : SPI1_mosi

 

Thank you.

2 REPLIES 2
mfgkw
Senior III

Looks fine.

Mahmoud Ben Romdhane
ST Employee

Hello @@CabinJo 

Let me thank you for posting and welcome to the ST Community.

I recommend that you take a look at the examples provided through the STM32Cube_FW_G0_V1.6.2 firmware package under this path: 

C:\Users\_\STM32Cube\Repository\STM32Cube_FW_G0_V1.6.2\Projects\NUCLEO-G070RB\Examples\SPI

Thanks.

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.