2026-06-01 1:47 AM - last edited on 2026-06-01 2:38 AM by Andrew Neil
Two independent outputs have been configured in HRTIM, but the trigger source for the second output cannot be set, indicating that it must be 0.
HRTIM中已经设置了两路独立输出,第二路无法设置触发源,提示必须是0
Two independent outputs have been configured in HRTIM, but the trigger source for the second output cannot be set, indicating that it must be 0.
2026-06-01 2:04 AM
Hello @xiaowenbin
Thank you for posting!
This is a known issue and has been already reported to dedicated team as discussed under this thread: Solved: HRTIM configuration when updated to 6.16.1 CubeMX - STMicroelectronics Community
BR, Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.