2026-02-03 10:44 PM - last edited on 2026-02-13 7:18 AM by Andrew Neil
I generated a project using STM32CubeMX for the STM32N6570-DK board.
Steps performed:
Generated code using CubeMX (default configuration)
Imported project into STM32CubeIDE
Built the project successfully (no build errors)
Attempted to run/debug the application
During programming / start of execution, the debugger stops with the following message:
Break at address “0x18003A1A” with no debug information available, or outside of program code
2026-02-12 7:42 AM
Hello @MownishBugatha
Please provide more details (CubeMx and firmware version used) , which project used. If possible, share your ioc file.
How to write your question to maximize your chances to find a solution