cancel
Showing results for 
Search instead for 
Did you mean: 

The exe-config node can't extract variable from elf file

NChan.7
Associate

Hello, I followed the tutorial with just one variable (extracted from an elf) there was no problem the variable showed in the chart. But when I added another variable to the code and got a new elf. I went to the variable node to add the new variable but there's none (the first variable also gone). I tried with other elf files from other projects but it doesn't work either. Thank you in advance! (I'm using the CubeMonitor in Window10)

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Closing the ticket as no update since a while

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Richard.Chvr
ST Employee

Hello @NChan.7​ 

Can you share your flow and elf file if possible.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Closing the ticket as no update since a while

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.