2025-03-11 3:57 AM - last edited on 2025-03-12 3:14 AM by STTwo-32
Hello
i'm using STM32WB05KZ (nucleo board) : Nucleo-WB05KZ with STM32CubemonitorRF
Please why here i can't select "Get RSSI" , it's locked ?
and other question how can i modifie the outpout power (TX) of the antenna ( dBm) ?
thank you
2025-03-12 3:12 AM
Hello @ljm
The Get RSSI option is locked due to the Firmware implementation on the STM32WB0, the ACI_HAL_READ_RSSI command is not supported.
For the second question, if you are testing on a transmitter, you can set the PA Level you want here:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-12 3:31 AM - edited 2025-03-12 3:32 AM
hello
thanks for replying.
for "Get RSSI" means there is no solution to get the RSSI value ?
i do the some in mode transmission, i get the number of packets but there is no value for the rssi :
thanks
2025-03-12 3:34 AM - edited 2025-03-12 3:37 AM
For the STM32WB0, you can't get the RSSI using the STM32CubeMonitorRF.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.