Solved
Setupstm32cubemonitorpower crash
Hi,
I'm using a fresh debian testing (12) and when i try to launch "SetupSTM32CubeMonitor-Power.jar", i get the error :
Command line arguments:
SEVERE: java.lang.ArrayIndexOutOfBoundsException: Index 70131 out of bounds for length 22674Debian is not in the supported operating system, but ubuntu should not be so far. I found on the forum, that the error occured on stm32cubemonitor on ubuntu recent version.
Is there a patch/upgraded planned or anyway to make it run ?
Could someone on ubuntu tell me if it work on it ?
Thanks in advance,