2021-08-02 04:19 AM
I have multiple linear charts on my Dashboards and would like to zoom them all identically on the X axis. Is it possible to inject a ui_control message to modify the Xmin and Xmax values?
It would be great to have a feature that would allow sync'ing the X zoom factor and Xmin values over a chart group.
Best regards.
Jean-Daniel
Solved! Go to Solution.
2021-08-04 03:28 AM
Hello Jean-Daniel
Unfortunately, for the moment, it is not possible to synchronize Xvalues between different charts.
Sorry for the inconvenience.
2021-08-04 03:28 AM
Hello Jean-Daniel
Unfortunately, for the moment, it is not possible to synchronize Xvalues between different charts.
Sorry for the inconvenience.
2021-08-05 09:57 PM
It's a pitty that it's not possible. if https://community.st.com/s/ideazone would have a STMCubeMonitor dedicated section, I would add this as an improvement idea. If I'm correct, the original NodeRed graph allows to modify the Xmin and Xmax properties at runtime. STM chart component should provide the same feature.
Best regards.
Jean-Daniel
2021-08-06 02:57 AM
Thanks for this improvement idea, we will check whether it is possible to implement it.
Richard