cancel
Showing results for 
Search instead for 
Did you mean: 

Wrong version number of CubeIde shown

LMI2
Lead

I have CubeIde 1.61 installed on Win10/64 hard disk. About box/dialog says it is version 1.61, that is, the current version. Desktop icon or shortcut says it is version 1.40 or something. That is the original version number I installed sometime ago and then later updated.

I can change the name easily, so that is not the problem. Perhaps the shortcut should only be named CubeIde?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Pavel A.
Super User

This is a known issue. TL;DR not a bug, won't be fixed.

Instead, to know what is the true version (besides the About dialog), open the file stm32cubeide.ini in the CubeIDE dir.

Look for line like:

-Declipse.buildId=Version 1.6.0

This gives the actual version.

--pa

View solution in original post

4 REPLIES 4
Pavel A.
Super User

This is a known issue. TL;DR not a bug, won't be fixed.

Instead, to know what is the true version (besides the About dialog), open the file stm32cubeide.ini in the CubeIDE dir.

Look for line like:

-Declipse.buildId=Version 1.6.0

This gives the actual version.

--pa

LMI2
Lead

MS style: a feature, not a bug.

Piranha
Chief II

Polluting the user's Desktop and other private folders with shortcuts is actually a leftover from 90s, when it was "cool" to pollute everything with a zillion toolbars, pop-ups, shortcuts and whatnot.

https://github.com/postmanlabs/postman-app-support/issues/6604

@Piranha​ unfair & useless comment ...

STM32CubeIDE installer is asking you if you want or not shortcut setup ....