2020-09-29 12:31 PM
I usually copy the project folder from the workspace, delete the files from the Debug and Release folder, and compact in zip format.
I noticed that the project cleanup function does not clean both Debug and Release folders at the same time.
And I also noticed that the clean function is not very interesting to always do, because the compilation takes longer, especially if the IDE is still being used.
I'm asking this, because I had backups of 20MB each, which amounted to 1GB, and after cleaning the Debug and Release folders, the files only occupied 150MB.
Due to the files being compressed and using Linux, I was able to clean the Debug and Release folders with this command:
$for i in *;do zip -d "$i" USB_HOST_HID*/Debug/\* USB_HOST_HID*/Release/\*; doneNote: USB_HOST_HID = my project folder
Is there an automatic way to backup the projects?
2020-09-29 1:28 PM
Version control tools such as git exist specially for this.
If you keep the project in git: open a terminal and type:
git archive --format zip -o [zip_file_name] HEAD
and it will create a nice zip archive for you. Only with files that are checked in, no garbage,
-- pa
2020-09-29 10:10 PM
Most probably Eclipse native File>Export>Archive File is doing job for you.
About clean target ... such is working per active build configuration so no cleaning Debug and Release at once is common Eclipse behavior.