2026-04-16 5:13 AM - last edited on 2026-04-16 8:22 AM by Andrew Neil
In the "Debug Configurations" window (or at least that is the only place I have verified it so far), when scrolling down to access the options at the bottom, the mouse pointer might accidentally hover over a combo box. If you continue scrolling, the combo box cycles through its options down to the last value before the main window continues to scroll.
This can cause (and has caused me) quite a few headaches while debugging one of my projects.
I believe the correct approach would be to disable this scrolling behavior for combo boxes to prevent accidental changes.
Best regards!
2026-04-16 7:55 AM - edited 2026-04-20 3:29 AM
Hello @giuliano2505
Thank you for highlighting this issue,
I will raise it internally to the dedicated team to see if there is a possibility of such a request. Internal ticket number: CDM0061930 (This is an internal tracking number and is not accessible or usable by customers.)
BR, Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.