cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to flash Nucleo-H563ZI with STM32CubeIDE V1.14

Nikita91
Lead II

I wanted to use a Nucleo-H563ZI but I can’t program it:

STMicroelectronics ST-LINK GDB server. Version 7.5.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.

Starting server with the following options:
        Persistent Mode            : Disabled
        Logging Level              : 1
        Listen Port Number         : 61234
        Status Refresh Delay       : 15s
        Verbose Mode               : Disabled
        SWD Debug                  : Enabled
        InitWhile                  : Enabled

Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Shutting down...
Exit.



Error in final launch sequence:

Failed to execute MI command:
target remote localhost:61234

Error message from debugger back end:
localhost:61234: Connection timed out.
Failed to execute MI command:
target remote localhost:61234

Error message from debugger back end:
localhost:61234: Connection timed out.
localhost:61234: Connection timed out.

STLINK firmware version: V3J13M4

But with STM32CubeProgrammer it works. So it seems to me that the board and the STLINK are in working order.

After several tests with my application, I made a cleaning:

  • Uninstall STM32CubeProgrammer and STM32CubeIDE
  • Install STM32CubeIDE 1.14
  • Install STM32CubeProgrammer 2.15
  • Create a new workspace
  • Import a simple example of the H5 package: GPIO_IOToggle

Compilation OK, but flash download impossible.

But STM32CubeProgrammer  works and the LEDs blinks.

 

I also have a Nucleo-H723 board with a STLINK V3 (but seems to be a different version than that of the H563 board) => Doesn't work either (With the same version of STLINK firmware: V3J13M4)

But download and debug work on the H723 board with TrueSTUDIO. So the board works.

 

What's stopping me from using these boards with STM32CubeIDE?

 

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Nikita91
Lead II

Hello,

Attached are the gdbserver log I get. This log makes me think that the drivers are installed and working, at least a little.

To get this log I used a Nucleo board as STLINK bridge.

I get exactly the same trace wit a STLINK_V3MODS.

The connection fails (accept after timeout!):

[0.186] WaitConnection():  Waiting for connection on port 61234...
[0.193] WaitConnection():  Waiting for connection on port 61235...
[18.327] WaitConnection():  Accepted connection on port 61234...
[18.329] WaitConnection():  Waiting for connection on port 61234...