cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32wle5jci6

Nani96
Associate II

I have been working in Stm32wle5jci6,im trying to integrate My I2C code with lorawan code package downloaded from github. I had tested with Macros in that case the data was pushed in Chripstack, but whenever i try to connect the sensor i am unable to read the sensor data. Note : im using HTU31D sensor and its working. 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello @Nani96 ,

Did you manage to get a communication with your board?

When you debug your project, where the code hangs/stop?

Maybe need check your device configuration.

It will be better to attach your code and error message, this will help community users to help you.

 Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

2 REPLIES 2
Imen.D
ST Employee

Hello @Nani96 ,

Did you manage to get a communication with your board?

When you debug your project, where the code hangs/stop?

Maybe need check your device configuration.

It will be better to attach your code and error message, this will help community users to help you.

 Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Nani96
Associate II

static void SendTxData(void)

{

uint16_t pressure = 0;

int16_t temperature = 0;

sensor_t sensor_data;

UTIL_TIMER_Time_t nextTxIn = 0;

 

#ifdef CAYENNE_LPP

uint8_t channel = 0;

#else

uint16_t humidity = 0;

uint32_t i = 0;

int32_t latitude = 0;

int32_t longitude = 0;

uint16_t altitudeGps = 0;

#endif /* CAYENNE_LPP */

 

// EnvSensors_Read(&sensor_data);

temperature = (SYS_GetTemperatureLevel() >> 8);

pressure = (uint16_t)(sensor_data.pressure * 100 / 10); /* in hPa / 10 */

float Temp = Get_temperature(); // function reads temperature from sensor

AppData.Port = LORAWAN_USER_APP_PORT;

 

#ifdef CAYENNE_LPP

CayenneLppReset();

CayenneLppAddBarometricPressure(channel++, pressure);

CayenneLppAddTemperature(channel++, temperature);

CayenneLppAddRelativeHumidity(channel++, (uint16_t)(sensor_data.humidity));

 

if ((LmHandlerParams.ActiveRegion != LORAMAC_REGION_US915) && (LmHandlerParams.ActiveRegion != LORAMAC_REGION_AU915)

&& (LmHandlerParams.ActiveRegion != LORAMAC_REGION_AS923))

{

CayenneLppAddDigitalInput(channel++, GetBatteryLevel());

CayenneLppAddDigitalOutput(channel++, AppLedStateOn);

}

 

CayenneLppCopy(AppData.Buffer);

AppData.BufferSize = CayenneLppGetSize();

#else /* not CAYENNE_LPP */

humidity = (uint16_t)(sensor_data.humidity * 10); /* in %*10 */

 

AppData.Buffer[i++] = AppLedStateOn;

AppData.Buffer[i++] = (uint8_t)((pressure >> 8) & 0xFF);

AppData.Buffer[i++] = (uint8_t)(pressure & 0xFF);

AppData.Buffer[i++] = (uint8_t)(temperature & 0xFF);

AppData.Buffer[i++] = (uint8_t)((humidity >> 8) & 0xFF);

AppData.Buffer[i++] = (uint8_t)(humidity & 0xFF);

 

if ((LmHandlerParams.ActiveRegion == LORAMAC_REGION_US915) || (LmHandlerParams.ActiveRegion == LORAMAC_REGION_AU915)

|| (LmHandlerParams.ActiveRegion == LORAMAC_REGION_AS923))

{

AppData.Buffer[i++] = 0;

AppData.Buffer[i++] = 0;

AppData.Buffer[i++] = 0;

AppData.Buffer[i++] = 0;

}

else

{

latitude = sensor_data.latitude;

longitude = sensor_data.longitude;

 

AppData.Buffer[i++] = GetBatteryLevel(); /* 1 (very low) to 254 (fully charged) */

AppData.Buffer[i++] = (uint8_t)((latitude >> 16) & 0xFF);

AppData.Buffer[i++] = (uint8_t)((latitude >> 8) & 0xFF);

AppData.Buffer[i++] = (uint8_t)(latitude & 0xFF);

AppData.Buffer[i++] = (uint8_t)((longitude >> 16) & 0xFF);

AppData.Buffer[i++] = (uint8_t)((longitude >> 8) & 0xFF);

AppData.Buffer[i++] = (uint8_t)(longitude & 0xFF);

AppData.Buffer[i++] = (uint8_t)((altitudeGps >> 8) & 0xFF);

AppData.Buffer[i++] = (uint8_t)(altitudeGps & 0xFF);

}

 

AppData.BufferSize = i;

#endif /* CAYENNE_LPP */

 

if (LORAMAC_HANDLER_SUCCESS == LmHandlerSend(&AppData, LORAWAN_DEFAULT_CONFIRMED_MSG_STATE, &nextTxIn, false))

{

APP_LOG(TS_ON, VLEVEL_L, "SEND REQUEST\r\n");

}

else if (nextTxIn > 0)

{

APP_LOG(TS_ON, VLEVEL_L, "Next Tx in : ~%d second(s)\r\n", (nextTxIn / 1000));

}

}

hi, my Get_temperature function always reads 0 if i tried to implement the sensor code in lorawan package.

can any one tell me what was the issue with the code. Im transmitting data in cayenne format.