cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WL55JC1 Not Waking from Standby via RTC Alarm A

pavan1
Associate

Hi,

I'm facing an issue with waking the STM32WL55JC1 from Standby mode using RTC Alarm A.

Setup:

  • Using LSE as RTC clock source

  • RTC and Alarm A are initialized correctly

  • Alarm A interrupt works when not entering standby

  • Wake-up via RTC Wakeup Timer works fine (standby + timer = success)

Issue:

When I:

  1. Clear RTC time and date

  2. Set Alarm A to trigger a few seconds ahead

  3. Enter Standby mode

  4. Wait for wake-up

→ The system does not wake up from Alarm A.

However, if I skip Standby mode, Alarm A fires the interrupt as expected.

Observation:

  • RTC Alarm A interrupt is configured and enabled.

  • EXTI and NVIC settings are correct.

  • I suspect the Alarm A wakeup source isn’t properly enabled or EXTI line isn’t configured before entering standby.


    Request:

    Could you confirm the correct sequence or any missing configuration required for:

    • Enabling Alarm A as a wakeup source from standby

    • Ensuring EXTI line 17 is correctly set before standby

    Let me know if additional register dumps or code snippets are needed.

    Thanks,




0 REPLIES 0