cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407 - CMSIS DSP - IFFT not working with audio input/output

lukegalea16
Associate II
I'm currently using the stm32f407g-disc1 and reading an audio input through PMOD I2S2. I've carried out some examples and the hardware is working fine (writing data from the rx to the tx buffer) such as the code below.
 
```
for (int i=0; i<BUFFER_LENGTH*4; i=i+4) {
txBuf[i] = rxBuf[i];
txBuf[i+1] = rxBuf[i+1];
txBuf[i+2] = 0;
txBuf[i+3] = 0;
}
```
 
I now wish to perform the FFT on this incoming buffer, manipulate it (my first aim is to implement a pitch shifting algorithm) and perform the IFFT again. Thus I've tried the following:
 
```
for (int i=0; i<BUFFER_LENGTH*4; i=i+4) {
fft_in_buf[fft_in_ptr] = (float) ((int) (rxBuf[i]<<16)|rxBuf[i+1]);
fft_in_ptr++;
}
 
arm_rfft_fast_f32(&fft_handler, fft_in_buf, fft_out_buf, 0);
arm_rfft_fast_f32(&fft_handler, fft_out_buf, fft_in_buf, 1);
 
fft_in_ptr = 0;
 
for (int i=0; i<BUFFER_LENGTH*4; i=i+4) {
        txBuf[i] = (fft_in_buf[fft_in_ptr] >> 16) & 0xFF; // MSB
        txBuf[i + 1] = fft_in_buf[fft_in_ptr] & 0xFF;     // LSB
        txBuf[i + 2] = 0;
        txBuf[i + 3] = 0;
 
        fft_in_ptr++;
}
```
 
In the main initialization I'm also carrying out `arm_rfft_fast_init_f32(&fft_handler, BUFFER_LENGTH);`
 
 
My issue is that I get a very very low output (barely audible) with the above code. I might have a scaling issue as I found in similar issues but I still can't get it to work by scaling fft_in_buf[fft_in_ptr].
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hi, thank you for pointing me in the right direction. My issue was in fact with converting back the tx buffer.

 

for (int i=0; i<BUFFER_LENGTH*4; i=i+4) {
        txBuf[i] = (fft_in_buf[fft_in_ptr] >> 16) & 0xFFFF; // MSB
        txBuf[i + 1] = fft_in_buf[fft_in_ptr] & 0xFFFF;     // LSB
        txBuf[i + 2] = 0;
        txBuf[i + 3] = 0;

        fft_in_ptr++;
}

View solution in original post

3 REPLIES 3
AScha.3
Super User

You use a float fft , so scaling is not the problem, i suppose. (float giving about 1500 dB dynamic range)

What comes out, if you just comment out the two // arm_rfft_fast_f32()  lines ?

If you feel a post has answered your question, please click "Accept as Solution".

Hi, thank you for pointing me in the right direction. My issue was in fact with converting back the tx buffer.

 

for (int i=0; i<BUFFER_LENGTH*4; i=i+4) {
        txBuf[i] = (fft_in_buf[fft_in_ptr] >> 16) & 0xFFFF; // MSB
        txBuf[i + 1] = fft_in_buf[fft_in_ptr] & 0xFFFF;     // LSB
        txBuf[i + 2] = 0;
        txBuf[i + 3] = 0;

        fft_in_ptr++;
}
waclawek.jan
Super User

Thanks for coming back with the solution.

JW