cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Cube IDE could not save <Word document>

jlthompson
Senior

I added a folder called Docs to my project, then created release notes using Word and dropped in the newly created Docs folder. When I try to build, I get a message box:

jlthompson_0-1752102857444.png

How do I fix this?

1 ACCEPTED SOLUTION

Accepted Solutions

Doh! And a face palm, too!! At some point, I tried opening the Word document by double-clicking it; I vaguely remember that nothing happened. However, as I was closing editor tabs just now, I noticed an empty editor tab for the file, and an asterisk indicating that it needed to be saved. I closed the tab, without saving, of course, and now the project builds flawlessly. Sorry for the fire drill. 

View solution in original post

3 REPLIES 3
Karl Yamashita
Principal

What version STM32CubeIDE?

I was able to follow what you've done and I can build with no issues.

Show your project tree and where Docs and file is located.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

Thanks for the assistance, Karl. I'm running is:

STM32CubeIDE
Version: 1.19.0
Build: 25607_20250703_0907 (UTC)
OS: Windows 11, v.10.0, x86_64 / win32
Java vendor: Eclipse Adoptium
Java runtime version: 21.0.3+9-LTS
Java version: 21.0.3

My project tree is:

jlthompson_0-1752109255824.png

You can see 'Well Status Monitor Release Notes.docx' in the 'Docs' folder. I do not have Word open.

Doh! And a face palm, too!! At some point, I tried opening the Word document by double-clicking it; I vaguely remember that nothing happened. However, as I was closing editor tabs just now, I noticed an empty editor tab for the file, and an asterisk indicating that it needed to be saved. I closed the tab, without saving, of course, and now the project builds flawlessly. Sorry for the fire drill.