2025-07-03 3:12 AM
My code gets complied without any errors. But just before the uploading completes:
<signal handler> called at 0xfffffff9 is displayed.
Even though after that my code runs properly without any hardfault.
Solved! Go to Solution.
2025-07-03 6:49 AM
0xFFFFFFF9 suggests an interrupt is called but the interrupt table is incorrect or erased. Probably the debugger is in an intermediate state.
If things are working, I wouldn't bother with it.
2025-07-03 6:49 AM
0xFFFFFFF9 suggests an interrupt is called but the interrupt table is incorrect or erased. Probably the debugger is in an intermediate state.
If things are working, I wouldn't bother with it.