2025-11-27 4:50 AM
Created a number of files in your glorious new IDE.
After opening and closing a few projects in at attempt to find a hidden menu option, I can now see my .project files in finder but attempting to open them with the IDE via double clicking shows NO project data, just a blank space where the explorer should be.
Is this a design 'quirk' with an odd workaround where I can recover the file somehow?
is it an issue with V2.0.0 which needs resolving?
Or is it just an inevitable fact of dealing with this buggy rubbish software?
I actually wouldn't have minded MX moving to a different platform if it was designed to move the whole stack away from this eclipse junk, but I don't understand why you'd expend effort making IDE and MX less usable whilst not bothering to do anything about the buggy or just plain weird behaviour of the IDE
2025-11-27 4:58 AM - edited 2025-11-27 5:09 AM
Hello @adam_C
Thank you for posting
Could you please share a screenshot or a little video that illustrate this behavior ?
Also could you please provide more details about your OS?
Meanwhile I am checking this behavior. I will get back to you asap
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-11-27 5:01 AM
@adam_C wrote:move the whole stack away from this eclipse junk,
That's what the STM32CubeIDE for Visual Studio Code (MCUs) is all about...
2025-11-27 5:55 AM
2025-11-27 6:00 AM
2025-11-27 6:05 AM
Well, it seems for quite some time that the Mac platform is the red-haired stepchild of ST's software department.
But to be honest, Macs are an exotic occurence in the embedded software business. I never came across one in a professional environment.
2025-11-27 7:11 AM
I have to wonder what is going on inside MacOS (and Linux) that these issues keep happening. Eclipse has been around for quite a while. This isn't something special that ST is doing. What are they changing between versions that is causing stuff to break?
2025-11-27 8:15 AM
2025-11-28 1:39 AM
Hello @adam_C
Could you please clarify whether you are keeping your IDE open and simply opening or closing the project, or if you are actually restarting CubeIDE? Also, could you try opening CubeIDE in a new workspace to see if you encounter the same issue?
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.