cancel
Showing results for 
Search instead for 
Did you mean: 

NullPointerException in com.st.stm32cube.ide.mcu.toolchain.ui.ToolChainHelper

Avan .12
Associate III

I get the following exception when I try to debug en.fp-sns-allmems1:

!ENTRY org.eclipse.core.jobs 4 2 2023-03-15 11:08:42.955

!MESSAGE An internal error occurred during: "Launching SensorTile".

!STACK 0

java.lang.NullPointerException

at com.st.stm32cube.ide.mcu.toolchain.ui.ToolChainHelper.validateDebugLaunch(ToolChainHelper.java:38)

at com.st.stm32cube.ide.mcu.debug.launch.DSFDelegate.preLaunchCheck(DSFDelegate.java:100)

at org.eclipse.debug.internal.core.LaunchConfiguration.launch(LaunchConfiguration.java:767)

at org.eclipse.debug.internal.core.LaunchConfiguration.launch(LaunchConfiguration.java:716)

at org.eclipse.debug.internal.ui.DebugUIPlugin.buildAndLaunch(DebugUIPlugin.java:1021)

at org.eclipse.debug.internal.ui.DebugUIPlugin$2.run(DebugUIPlugin.java:1224)

at org.eclipse.core.internal.jobs.Worker.run(Worker.java:63)

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Avan .12
Associate III

Please ignore this question : i think it has something to do with me incorrectly connection the ST Link to the sensortile. ​

View solution in original post

4 REPLIES 4
Avan .12
Associate III

!SESSION 2023-03-15 11:04:31.296 -----------------------------------------------

eclipse.buildId=Version 1.12.0

java.version=11.0.17

java.vendor=Eclipse Adoptium

BootLoader constants: OS=win32, ARCH=x86_64, WS=win32, NL=nl_NL

Command-line arguments: -os win32 -ws win32 -arch x86_64

Semer CHERNI
ST Employee

Hello @Avan .12​ 

First let me thank you for posting.

I wonder if this behavior occur when debugging all your projects or just a specific one?

Could you import the project you are debugging into an other clean workspace and tell if the issue keep exiting?

BR,

Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Avan .12
Associate III

1) I updated stm32cubeide to latest 1.12 version

2) created a newIt clean workspace and

3) imported : https://www.st.com/en/embedded-software/fp-sns-allmems1.html

4) i am able to compile it successfully

5) when I hit debug button in stm32cubeide I get this exception immediately

project for sensor tile : https://www.st.com/en/evaluation-tools/steval-stlcs02v1.html

Cheers

Avan .12
Associate III

Please ignore this question : i think it has something to do with me incorrectly connection the ST Link to the sensortile. ​