cancel
Showing results for 
Search instead for 
Did you mean: 

Modbus over ethernet with multiple master at same time

CJ007
Associate II

Hi , I implemented modbus over ethernet on my NUCLEO-H723ZG mcu board. I could poll from modbus poll software. But when I try to poll from modbus poll from different devices at the same time , it is not able to poll.Couldn't connect.

3 REPLIES 3
Ozone
Lead II

There is very little information in your post, nobody can help you based upon that.

> Modbus over ethernet with multiple master at same time

I am not sure what this title is supposed to mean.
Modbus is specified as a single-master bus system.

> But when I try to poll from modbus poll from different devices at the same time , it is not able to poll.Couldn't connect.

Debug the low-level transmit routines, and record the actual bus transmissions with a separate tool (like Wireshark).
You need to know what exactly fails, and where.

Hello @Ozone  I tried to create an array of socket pointers in tcp stack and allowed connection of more than one master according to the size of array.Thus enabling multiple sockets in the pcbListen.  

Not sure if you mean to connect your device as a slave to multiple masters at the same time.
And I'm not sure if and how Modbus master can deal with other master on the same network. I haven't dealt with Modbus for quite a while now ...

But the recommendation for debugging the low-level routines and run a network monitoring software still stands.
BTW, Wireshark has a Modbus profile, and you can easily filter out the relevant packages for your environment.