Skip to main content
Associate III
November 27, 2024
Solved

Misalignment of Reset_Handler Address in Vector Table After Moving Flash Bank

  • November 27, 2024
  • 1 reply
  • 1011 views

I’m encountering an issue with my STM32H755 application after moving the flash memory to accommodate SBSFU. The Reset_Handler address in the vector table is misaligned by one flash bank. Here are the details:

Background:

  • Microcontroller: STM32H755
  • Bootloader: SBSFU
  • Development Environment: STM32CubeIDE1.12

Problem: After moving my application to start at 0x08020400 to make room for SBSFU, the Reset_Handler address in the vector table is incorrect. The address is off by 0x203FF.

Linker Script: Here is the relevant part of my linker script:

MEMORY
{
 FLASH (rx) : ORIGIN = 0x08020400, LENGTH = 896K
 RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 128K
 // Other memory regions
}

SECTIONS
{
 .isr_vector :
 {
 . = ALIGN(8);
 KEEP(*(.isr_vector))
 FILL(0);
 . = ORIGIN(FLASH) + LENGTH(FLASH) - 1;
 BYTE(0)
 . = ALIGN(8);
 } > FLASH

 .text :
 {
 . = ALIGN(4);
 *(.text)
 *(.text*)
 *(.glue_7)
 *(.glue_7t)
 *(.eh_frame)
 KEEP(*(.init))
 KEEP(*(.fini))
 . = ALIGN(4);
 _etext = .;
 } > FLASH

 // Other sections
}

Startup Code: Here is the relevant part of my startup assembly file:

Assembly
 
.section .isr_vector, "a", %progbits
.type g_pfnVectors, %object
.size g_pfnVectors, .-g_pfnVectors

g_pfnVectors:
 .word _estack
 .word Reset_Handler
 .word NMI_Handler
 .word HardFault_Handler
 // Other exception vectors

.thumb_func
.type Reset_Handler, %function
Reset_Handler:
 // Reset handler code
 b .
 

Vector Table Output: Here are the first 10 entries of the vector table:

0x08020400: 0x24020000
0x08020404: 0x080656E5
0x08020408: 0x08064549
0x0802040C: 0x0806454F
0x08020410: 0x08064555
0x08020414: 0x0806455B
0x08020418: 0x08064561
0x0802041C: 0x00000000
0x08020420: 0x00000000
0x08020424: 0x00000000

What I’ve Tried:

  • Verified the linker script and startup code.
  • Ensured the vector table is correctly placed at 0x08020400.
  • Checked the alignment and memory regions.

Question: Why is the Reset_Handler address in the vector table misaligned by one flash bank, and how can I fix this issue?

This topic has been closed for replies.
Best answer by tstokes

Resolved. 

The SBSFU postbuild script that generates the .sfb firmware requires both the elf and bin files. I had not updated one of these after updating the flash address. 

1 reply

tstokesAuthorBest answer
Associate III
November 27, 2024

Resolved. 

The SBSFU postbuild script that generates the .sfb firmware requires both the elf and bin files. I had not updated one of these after updating the flash address.