2025-06-03 3:09 PM
Hi. There is a minor bug in writing to LEDs when this package is used on the STM32H573I-DK development board.
In ..\Common\cli\logging.c there is the following code at line 77:
HAL_GPIO_WritePin( LED_RED_GPIO_Port, LED_GREEN_Pin, GPIO_PIN_SET );
HAL_GPIO_WritePin( LED_RED_GPIO_Port, LED_RED_Pin, GPIO_PIN_RESET );The first line has the wrong port specified. On boards with both LEDs on the same port this wouldn't be noticed, but on the STM32H573I-DK the LEDs are on different ports.
Solved! Go to Solution.
2025-06-03 4:25 PM - edited 2025-06-04 8:00 AM
Hello @ChrisF
It seems to be a Typo on the file. I’ve escalated this for correction on the future (under internal ticket number 211643).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-06-03 4:25 PM - edited 2025-06-04 8:00 AM
Hello @ChrisF
It seems to be a Typo on the file. I’ve escalated this for correction on the future (under internal ticket number 211643).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.