cancel
Showing results for 
Search instead for 
Did you mean: 

Issue with HAL_OSPIM_Config() function when using two OSPI ports

DWWelch
Associate III

Hello,

I noticed an issue with the HAL OSPIM initialization code when initializing two OSPI ports. The first port initializes correctly, but when initializing the second port the HAL_OSPIM_Config() function does not re-enable the first ports signal lines. So the second port works, but the first port signals are disabled. I am using STM32H7A3 MCU and STMCube STM32H7 V1.12.1.

Thanks,

Dan

2 REPLIES 2
Andrew Neil
Super User

Duplicate:

https://community.st.com/t5/stm32-mcus-products/both-octospi-ports-memory-mapped-on-stm32h7a3/td-p/837206 ?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Mahmoud Ben Romdhane
ST Employee

Hello @DWWelch ,

 

The same issue was already reported and raised to the development team under this internal ticket

(Ticket Number: 203289). I will keep you up to date when the problem is solved.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.