cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a way to stop STM32CubeIDE from collapsing the Project Explorer every time the project is built? This is an absolutely annoying "feature".

johnvs2525
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
TDK
Super User

Doesn't help you much, but it doesn't do so for me. I doubt it's intended. I'm on Win10, and have used many different IDE version.

If you feel a post has answered your question, please click "Accept as Solution".
johnvs2525
Associate II

If I have compilation errors that end the build process prematurely, mine doesn't do it either. Is it possible there is a project Properties setting that puts a command in the makefile that causes this action? I've looked around and can't find anything that looks like it would cause it.

johnvs2525
Associate II

I finally figured this out. In the project Properties dialog, go to the "C/C++ Build" pane and the "Refresh Policy" tab. My project was listed. I deleted it from the list (it was the only thing listed) and no more post build "refreshing", i.e. completely collapsing every project folder I had open.

Thanks!