2025-05-28 1:14 AM
I have started for integration of NUCLEO-L476RG board with X-NUCLEO-IKS02A1 expansion board for getting live values from the accelerometer, magnetometer and gyroscope.
Started from creating a project on STM32CubeIDE then selected X-CUBE-MEMS1 package, selected Board Extension IKS02A1, motion fusion library, gyroscope calibration, accelerometer calibration and magnetometer calibration libraries.
Also, enabled the CRC, SPI, I2C, USART in the configurations. When generated the code, motion_fx.h file generated.
So further I want to know what else libraries or header files I need to acheive my final goal, to get tje yaw, pitch, roll values when the board is tilted or moved or to calibrate them.