How to specify separate compile flags for C and C++ using clangd extension for Visual Studio Code?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-04-29 9:18 AM - edited 2023-11-20 6:47 AM
I struggle all day with configuring clangd extension for Visual Studio Code to be able to provide all code intelligence feature for STM32 project that was created with STM32CubeIDE.
I mean - it works. Kind of. I provided a ridiculous number of include directories, symbols and such (mostly copied from STM32CubeIDE), but the problem is some flags should be set differently for C and C++ files.
It seems like STM32CubeIDE does that somehow.
With clangd I figured out I can create compile_flags.txt file and point the clang extension to use that file (--compile-commands-dir=.vscode).
So here is the beginning of my compiler_flags.txt file:
-mcpu=cortex-m7
-std=gnu11
-std=gnu++17
-D__GNUC__
-DDEBUG
-DCORE_CM7
-DUSE_HAL_DRIVER
-DSTM32H745xx
#-U__clang__
-U_WIN32
-ffunction-sections
-fdata-sections
-fno-exceptions
-fno-rtti
-fno-use-cxa-atexit
-Wall
-Wno-unknown-pragmas
--specs=nano.specs
-mfpu=fpv5-d16
-mfloat-abi=hard
-mthumb
-IC:\ST\STM32CubeIDE_1.12.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\lib\gcc\arm-none-eabi\10.3.1\include
-IC:\ST\STM32CubeIDE_1.12.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\lib\gcc\arm-none-eabi\10.3.1\include-fixed
-IC:\ST\STM32CubeIDE_1.12.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\arm-none-eabi\include\c++\10.3.1
-IC:\ST\STM32CubeIDE_1.12.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\arm-none-eabi\include\c++\10.3.1\arm-none-eabi\thumb\v7e-m+dp\hard
-IC:\ST\STM32CubeIDE_1.12.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.200.202301161003\tools\arm-none-eabi\include
However, this produce errors like this:
You get the point, some flags should be provided for the C compiler, some for the C++ compiler. How to achieve that goal?
BTW, I tried to used Microsoft C++ extension first, but it failed miserably with code completion. It offered me symbols from the entire codebase, instead of symbols from the class I was editing.
For that matter clangd is amazingly good. Its code completions are better than those offered by STM32CubeIDE. The only problem are those spurious errors.
For now I don't intend to compile the code with VS Code, I'm just using it as an editor.
- Labels:
-
STM32CubeIDE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-04-29 1:39 PM - edited 2023-11-20 6:48 AM
I found a partial solution:
.vscode/settings.json:
{
"clangd.arguments": [
"--compile-commands-dir=.vscode",
"--enable-config"
],
"clangd.onConfigChanged": "restart",
}
.clangd:
CompileFlags:
Add:
- "-mcpu=cortex-m7"
- "-DDEBUG"
- "-DCORE_CM7"
- "-DUSE_HAL_DRIVER"
- "-DSTM32H745xx"
- "-D__GNUC__"
- "-U_WIN32"
- "-ffunction-sections"
- "-fdata-sections"
- "-mfpu=fpv5-d16"
- "-mfloat-abi=hard"
- "-mthumb"
- "-Wall"
- "-Wno-unknown-pragmas"
- "--specs=nano.specs"
---
If:
PathMatch: [.*\.c, .*\.h]
CompileFlags:
Add:
- "-std=gnu11"
- "-I/source/embedded/stm32-gnu-tools/arm-none-eabi/include"
- "-I/source/embedded/stm32-gnu-tools/lib/gcc/arm-none-eabi/10.3.1/include"
- "-I/source/embedded/stm32-gnu-tools/lib/gcc/arm-none-eabi/10.3.1/include-fixed"
---
If:
PathExclude: [.*\.c, .*\.h]
CompileFlags:
Add:
- "-std=gnu++17"
- "-fno-exceptions"
- "-fno-rtti"
- "-fno-use-cxa-atexit"
- "-I/source/embedded/stm32-gnu-tools/arm-none-eabi/include"
- "-I/source/embedded/stm32-gnu-tools/arm-none-eabi/include/c++/10.3.1"
- "-I/source/embedded/stm32-gnu-tools/arm-none-eabi/include/c++/10.3.1/arm-none-eabi/thumb/v7e-m+dp/hard"
File .vscode/compile_flags.txt contains only my project include paths.
Most of the files are processed without errors, however, I still get something like this: