cancel
Showing results for 
Search instead for 
Did you mean: 

How to solve "Break at address "0xnnnnnnnn" with no debug information..."?

White_Fox
Associate III

Hi guys

My software compiles fine. But if I try to run or debug it, it ends up with this message:

 

Break at address "0xf3af4804" with no debug information available, or outside of program code.

 

The console output is this:

 

STMicroelectronics ST-LINK GDB server. Version 7.8.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.

Starting server with the following options:
        Persistent Mode            : Disabled
        Logging Level              : 1
        Listen Port Number         : 61234
        Status Refresh Delay       : 15s
        Verbose Mode               : Disabled
        SWD Debug                  : Enabled
        InitWhile                  : Enabled

Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
      -------------------------------------------------------------------
                       STM32CubeProgrammer v2.17.0                  
      -------------------------------------------------------------------



Log output file:   C:\Users\Oli\AppData\Local\Temp\STM32CubeProgrammer_a32392.log
ST-LINK SN  : 48FF6B064886575306321587
ST-LINK FW  : V2J45S7
Board       : --
Voltage     : 3.34V
SWD freq    : 4000 KHz
Connect mode: Under Reset
Reset mode  : Hardware reset
Device ID   : 0x438
Revision ID : Rev Z
Device name : STM32F303x4-x6-x8/F328xx/F334xx
Flash size  : 64 KBytes
Device type : MCU
Device CPU  : Cortex-M4
BL Version  : 0x50


Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a32392.srec
  File          : ST-LINK_GDB_server_a32392.srec
  Size          : 96.00 B 
  Address       : 0x08000000 


Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Download in Progress:


File download complete
Time elapsed during download operation: 00:00:00.101


Verifying ...


Download verified successfully 


Shutting down...
Exit.

 

Does anyone have an idea how to solve this? I'm just out of any ideas.

2 REPLIES 2
White_Fox
Associate III

Ok, I do not know what went wrong, but I could solve it with that way:

The project was generated from CubeMX. I just savecopied my source code and header files, and deleted everthing except the .ioc file from CubeMX.

After this, I just let CubeMX generate the project again. Pasting the source code and header files again and it works now fine again.

 

It is the big hammer method, but it is fast if you do not need to set up much extra stuff.

It just means the processor faulted at some address outside the scope of your source code.

Say it popped the bytes from an ASCII string in the PC or LR registers, ie 0x454E4E36. Or you're executing in ROM, ie 0x1FFFxxxx

Debug it, look critically at the code it has to execute, starting from Reset_Handler, perhaps disassemble and disect the code if necesary. Turn off "Run to main()" and step your way there from the code that executes first.

Inspect the Stack, try to unpick the call tree.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..