cancel
Showing results for 
Search instead for 
Did you mean: 

How to Debug at custom Start Address in STM32CUBEIDE?

ikassma
Senior

I am using stm32cubeide 1.12.1 version.

Debugging was attempted at the start address of the program, 0x08020000. The first download was completed and debugging was normally performed. However, if you press the reset button of stm32cubeide, the timer interrupt without a source continues to operate and is not normally executed.

If you change the start address of the program to 0x08000000, everything works normally.

Is there any other way to use the reset button of stm32cubeide normally at the start address of a randomly designated program?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Pavel A.
Super User

Very simple, just put the start address (or vectors address) in the debugger settings-> startup.

But after the reset the ST debugger won't automatically jump to the same start address again.

You have to break on the reset event and go the start address manually.

(other debuggers such as IAR behave differently)

Or you can burn a simple "bootloader" at 0x08000000 which just jumps to your app start address.

View solution in original post

4 REPLIES 4
Pavel A.
Super User

Very simple, just put the start address (or vectors address) in the debugger settings-> startup.

But after the reset the ST debugger won't automatically jump to the same start address again.

You have to break on the reset event and go the start address manually.

(other debuggers such as IAR behave differently)

Or you can burn a simple "bootloader" at 0x08000000 which just jumps to your app start address.

RetroInTheShade
Associate III

As an alternative, you can create a debug profile which excludes build and load… not as fast as reset but close.

How to set start address manually at reset event?

Uncheck "resume" in debug settings-> startup.

When the debugger stops at the CPU reset, find the desired start address in disassembly and "move" to it, or change the PC register in Registers view.