2020-03-10 2:30 AM
I've just started my first FreeRTOS-based project.
In the debugger, when I pause execution, all I see is this stack trace:
Thread #1 [main] 1 [core: 0] (suspended : Signal : 0:Signal 0)
prvCheckTasksWaitingTermination() at tasks.c:2,488 0x800b4f4
prvIdleTask() at tasks.c:3,235 0x800b404
pxPortInitialiseStack() at port.c:214 0x00ba94In order to be able to develop a FreeRTOS-based project, I need to be able to see the whole program, not just the currently suspended thread.
Is there a way, in CubeIDE, of turning on FreeRTOS debugging features such as those present in Atollic or Kinetis Design Studio?
http://blog.atollic.com/how-to-debug-freertos-projects-on-arm-cortex-m-devices
https://mcuoneclipse.com/2017/03/18/better-freertos-debugging-in-eclipse/
Solved! Go to Solution.
2020-03-10 6:27 AM
CubeIDE does not yet support the freeRTOS eclipse plugins. I think some persons have been able with third party plugins but not sure which ones.
source :
https://blog.st.com/stm32cubeide-free-ide/
If you need freeRTOS plugins you better stay with TrueStudio for now.
2020-03-10 6:27 AM
CubeIDE does not yet support the freeRTOS eclipse plugins. I think some persons have been able with third party plugins but not sure which ones.
source :
https://blog.st.com/stm32cubeide-free-ide/
If you need freeRTOS plugins you better stay with TrueStudio for now.
2020-03-10 6:50 AM
Thanks, I've successfully installed https://www.highintegritysystems.com/down-loads/stateviewer-plug-in/ into CubeMX 1.2.1, which provides panels for tasks, queues and timers, but not semaphores.
I assume the only way of seeing the other tasks' stacks/variables is to set a breakpoint in those tasks.